LS1021A SEC CRCA Dynamic Custom Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021A SEC CRCA Dynamic Custom Mode

ソリューションへジャンプ
3,612件の閲覧回数
Xi-nanWang
Contributor II

LS1021A, I use SEC for hardware CRC calculation, I can only run the STANDARD IEEE and IETF mode correctly, when it comes to Dynamic CUSTOM mode, the hardware will generate all ZERO results. The register configuration are the same except the mode selection AAI and Key Register. Did I miss any critical register bits? Or which registers should I consider to use CRCA dynamic custom mode?

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
3,462件の閲覧回数
bpe
NXP Employee
NXP Employee

Generating CRC with custom polynomials require a Job Descriptor that
is not in the standard JD library. Customers requiring custom crypto
operation descriptors are advised to request them through NXP
paid Professional Services:

Commercial Support and Engineering Services | NXP 

Regards,

Platon

元の投稿で解決策を見る

4 返答(返信)
3,463件の閲覧回数
bpe
NXP Employee
NXP Employee

Generating CRC with custom polynomials require a Job Descriptor that
is not in the standard JD library. Customers requiring custom crypto
operation descriptors are advised to request them through NXP
paid Professional Services:

Commercial Support and Engineering Services | NXP 

Regards,

Platon

3,462件の閲覧回数
Xi-nanWang
Contributor II

Resently I have encountered some problems when using SEC to calculate MD5. Since the source data size is too too big, i hope to splite it into chunks and calculate in times. Which registers should i concerned about and how to config? or does it need some sort of paid services again? 

0 件の賞賛
返信
3,462件の閲覧回数
Xi-nanWang
Contributor II

Thx a lot.

0 件の賞賛
返信
3,462件の閲覧回数
Xi-nanWang
Contributor II

Nobody has any clue? Or my statement is too vague? Any answer would help.

0 件の賞賛
返信