LS1021A Part Marking and System Version Register Value

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021A Part Marking and System Version Register Value

ソリューションへジャンプ
3,063件の閲覧回数
thomastamandl
Contributor I

Hi all,

on my board I am using a LS1021AXN7KQB, which is also the part marking. But U-Boot reports the following:

U-Boot 2015.01+SDKv1.9+geb3d4fc

CPU:   Freescale LayerScape LS1020, Version: 2.0, (0x87001020)

As the CAN interfaces are working, is there the possibility that a wrong value is stored in the system version register value? Might there be a problem where I schoud be aware of? According to the chip errata the system version register value shoud be 8700_1120h.

Best Regards

Thomas

ラベル(1)
0 件の賞賛
返信
1 解決策
2,933件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

According to Device Errata document you referring, the value 0x87001020 means your LS1021A device is incorrectly detected as LS1020A device. This usually happens when device personalization pins are not connected as required in device datasheet.

Please look LS1021A Data Sheet, Table 1, note 21 below this Table.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,934件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

According to Device Errata document you referring, the value 0x87001020 means your LS1021A device is incorrectly detected as LS1020A device. This usually happens when device personalization pins are not connected as required in device datasheet.

Please look LS1021A Data Sheet, Table 1, note 21 below this Table.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,934件の閲覧回数
thomastamandl
Contributor I

Thank you. Can you add Note 21 to the QSPI section in Table 1 too?

0 件の賞賛
返信
2,934件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Yes, I will notify documentation team, thank you for pointing.

0 件の賞賛
返信