LS1021A PLL setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021A PLL setting

4,829 Views
deepaknaiknavar
Contributor II

Hi,

I am evaluating LS1021A for one of our project.

Does code warrior provide option of performing PLL settings for all interfaces like DDRclk, Sysclk etc.?

I see SerDes Configuration and Validation is the tool for the same. If yes, then is it free or do we need to purchase it?

Thanks,

Deepak.

Labels (1)
Tags (1)
6 Replies

4,727 Views
pranavmadhu
Contributor IV

Hi Deepak,

You have to download 'CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA' to modify clock settings from reset configuration word(RCW). You can modify PLL config in RCW using the codewarrior tool. For more details about codewarrior tool refer

CodeWarrior ARMv8 64 bit |NXP

http://www.nxp.com/files/soft_dev_tools/doc/fact_sheet/LSARMv8ISAFS.pdf?fasp=1&WT_TYPE=Fact%20Sheets...

0 Kudos
Reply

4,728 Views
ufedor
NXP Employee
NXP Employee

> You have to download 'CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA'

This statement is not correct because LS1021A belongs to ARMv7.

0 Kudos
Reply

4,727 Views
pranavmadhu
Contributor IV

Hi Ufedor,

Thank you for correcting me. I'm having ubuntu 12.04 machine. I've attached a screen shot of the code warrior tool that I use. temp.png

In this it is displayed that ARM V8 ISA, and the pbl generated for qspi using this version works for my LS1021A-IOT board.

0 Kudos
Reply

4,727 Views
ufedor
NXP Employee
NXP Employee

The same QCVS is used by ARMv7 and ARMv8 CodeWarrior IDEs.

4,727 Views
deepaknaiknavar
Contributor II

Thanks Ufedor and Pranav,

0 Kudos
Reply

4,727 Views
ufedor
NXP Employee
NXP Employee

The request is not clear - is it about RCW preparation?

0 Kudos
Reply