LS1021A PCIe Wifi Interface Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021A PCIe Wifi Interface Issue

1,518件の閲覧回数
jiye
Contributor V

Anyone knows what's the issue here.

My kernel does have the interface up

But after I scan there are no wifi names showing up

pastedImage_1.png

pastedImage_1.png

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,425件の閲覧回数
bpe
NXP Employee
NXP Employee

This is a  device-specific problem, which, based on the provided screen
captures, is a result of device's failure to respond to certain commands.
This is totally the driver and underlying HW specific, thus the suggestion
is to approach your radio card manufacturer for more detailed error output
interpretation and troubleshooting.


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信