LS1021A - Any plans for a lidded package

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021A - Any plans for a lidded package

ソリューションへジャンプ
2,551件の閲覧回数
nikhilrao
Contributor II

Are there any plans for releasing the LS1021A in a lidded package, for use in an automative or outdoor industrial environment?

We have a robust passive heat sink solution worked out for use with the LS1021A's 525-pin FC-PBGA lidless package.  However we have concerns about moisture ingress and possible damage this may cause to a processor in lidless form.  Normally we conformally coat all our circuit boards (PCBAs) before mounting them in their enclosures or in certain cases completely seal the modules (housing the circuit boards) to IP65 rating. 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,376件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

There are no plans to offer LS1021A's in a lidded package.


Have a great day,
Andrei

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,377件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

There are no plans to offer LS1021A's in a lidded package.


Have a great day,
Andrei

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------