LS1021 NAND driver does not report bit flips

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021 NAND driver does not report bit flips

1,682 Views
keestrommel
Contributor IV

The LS1021A NAND driver provided in the QorIQ Linux SDK does nor report bit flips when bits are flipped in a sector of page. This applies both to U-Boot and Linux driver.

E.g. the following u-boot command returns OK while page 3fe000 contains an uncorrectable number of bit flips:

=> nand read 81000000 3fe000 1000

NAND read: device 0 offset 0x3fe000, size 0x1000
4096 bytes read: OK

Labels (1)
0 Kudos
Reply
1 Reply

1,510 Views
keestrommel
Contributor IV

The root cause of this problem is that the "struct fsl_ifc_nand" does not match the register map defined in the LS1021A Rev 1 reference manual. A boot that include a patch for this issue reports an error for a page with an uncorrectable number of bit flips, see:

=> nand read 81000000 3fe000 1000

NAND read: device 0 offset 0x3fe000, size 0x1000
NAND read from offset 3fe000 failed -74
0 bytes read: ERROR

The U-Boot patch file:

From 5d30cbefe1204be348af860591e2f3e97dc67286 Mon Sep 17 00:00:00 2001
From: Kees Trommel <[email protected]>
Date: Tue, 15 Nov 2016 16:16:00 +0100
Subject: [PATCH] fsl_ifc_nand-u-boot

Signed-off-by: Kees Trommel <[email protected]>
---
include/fsl_ifc.h | 9 ++++-----
1 file changed, 4 insertions(+), 5 deletions(-)

diff --git a/include/fsl_ifc.h b/include/fsl_ifc.h
index a86f216..6d1dc23 100644
--- a/include/fsl_ifc.h
+++ b/include/fsl_ifc.h
@@ -883,15 +883,14 @@ struct fsl_ifc_nand {
u32 nand_evter_en;
u32 res17[0x2];
u32 nand_evter_intr_en;
- u32 nand_vol_addr_stat;
- u32 res18;
+ u32 res18[0x2];
u32 nand_erattr0;
u32 nand_erattr1;
u32 res19[0x10];
u32 nand_fsr;
- u32 res20[0x3];
- u32 nand_eccstat[6];
- u32 res21[0x1c];
+ u32 res20;
+ u32 nand_eccstat[4];
+ u32 res21[0x20];
u32 nanndcr;
u32 res22[0x2];
u32 nand_autoboot_trgr;
--
2.5.5

The Linux patch file:

From c3ec47854734293594b11b8e88bb2179804935e4 Mon Sep 17 00:00:00 2001
From: Kees Trommel <[email protected]>
Date: Tue, 15 Nov 2016 16:19:09 +0100
Subject: [PATCH] fsl_ifc_nand-linux

Signed-off-by: Kees Trommel <[email protected]>
---
include/linux/fsl_ifc.h | 9 ++++-----
1 file changed, 4 insertions(+), 5 deletions(-)

diff --git a/include/linux/fsl_ifc.h b/include/linux/fsl_ifc.h
index 1770224..d48b886 100644
--- a/include/linux/fsl_ifc.h
+++ b/include/linux/fsl_ifc.h
@@ -729,15 +729,14 @@ struct fsl_ifc_nand {
__be32 nand_evter_en;
u32 res17[0x2];
__be32 nand_evter_intr_en;
- __be32 nand_vol_addr_stat;
- u32 res18;
+ u32 res18[0x2];
__be32 nand_erattr0;
__be32 nand_erattr1;
u32 res19[0x10];
__be32 nand_fsr;
- u32 res20[0x3];
- __be32 nand_eccstat[6];
- u32 res21[0x1c];
+ u32 res20;
+ __be32 nand_eccstat[4];
+ u32 res21[0x20];
__be32 nanndcr;
u32 res22[0x2];
__be32 nand_autoboot_trgr;
--
2.5.5

0 Kudos
Reply