LS1012A - eMMC memory support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1012A - eMMC memory support

2,556 次查看
markopavlovic
Contributor I

Can you please recommend eMMC memory which will work properly on LS1012A platform?

As I saw in the data brief, the parameters are following:

Interface on the LS1012A: eSDHC2

eMMC version: eMMC 4.4, eMMC 4.5

1.8V eMMC – modes FS/HS/HS200 or DDR

 

Can you please confirm this? Did you have chance to use the eMMC with LS1012A already? If yes, can you recommend some eMMC part number compatible with LS1012A?

标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

2,115 次查看
Pavel
NXP Employee
NXP Employee

There is no recommended eMMC for the LS1012A.

The LS1012a SDHC controller is the same as the LS1021a or LS1043a SDHC controller.

You can see in community that there is no information about problem the SDHC using on the LS1021a or LS1043a or LS1012a board.

For example the LS1021a QDS board uses the following eMMC:

MTFC4GMZDM-1M WT or KLMAG2GE2A-A001 or N2M400FDB311A3CF.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,115 次查看
jiye
Contributor V

Hi Pavel,

Do you think SLC or MLC, which one would be better fit for ls1021a

0 项奖励
回复