LS1012A PFE in phy-less direct mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1012A PFE in phy-less direct mode

Jump to solution
2,909 Views
dolphin1
Contributor I

Hi,

Will the pfe support making a phy-less connection from the LS1012A pfe to a Ethernet switch (VSC7421) in SGMII direct mode? https://www.kernel.org/doc/Documentation/devicetree/bindings/net/fixed-link.txt

|———————————|                                         |——————————|

|                                    —|———— SGMII ————|—                                |

|             LS1012A            |                                         |         VSC7421           |

|———————————|                                         |——————————|

                                                   NO MDIO

Thanks!

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,616 Views
ufedor
NXP Employee
NXP Employee

Technically, direct MAC-to-MAC connection over SGMII is possible for the LS1012A.

The PFE is not aware about the external connection type.

Refer to the QorIQ LS1012A Reference Manual, 28.5.13 Protocol Configuration Register 8 (PCCR8):
"Field
SGMIIA_KX
SGMIIb 1000Base-KX Configuration:

Note: this configuration bit must be set before performing any MDIO initialization of the PCS.
0b - SGMII mode
1b - 1000Base-KX mode"

View solution in original post

0 Kudos
Reply
2 Replies
2,616 Views
dolphin1
Contributor I

Ok. Thanks!

0 Kudos
Reply
2,617 Views
ufedor
NXP Employee
NXP Employee

Technically, direct MAC-to-MAC connection over SGMII is possible for the LS1012A.

The PFE is not aware about the external connection type.

Refer to the QorIQ LS1012A Reference Manual, 28.5.13 Protocol Configuration Register 8 (PCCR8):
"Field
SGMIIA_KX
SGMIIb 1000Base-KX Configuration:

Note: this configuration bit must be set before performing any MDIO initialization of the PCS.
0b - SGMII mode
1b - 1000Base-KX mode"

0 Kudos
Reply