LS1012A PFE in phy-less direct mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1012A PFE in phy-less direct mode

ソリューションへジャンプ
2,911件の閲覧回数
dolphin1
Contributor I

Hi,

Will the pfe support making a phy-less connection from the LS1012A pfe to a Ethernet switch (VSC7421) in SGMII direct mode? https://www.kernel.org/doc/Documentation/devicetree/bindings/net/fixed-link.txt

|———————————|                                         |——————————|

|                                    —|———— SGMII ————|—                                |

|             LS1012A            |                                         |         VSC7421           |

|———————————|                                         |——————————|

                                                   NO MDIO

Thanks!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,618件の閲覧回数
ufedor
NXP Employee
NXP Employee

Technically, direct MAC-to-MAC connection over SGMII is possible for the LS1012A.

The PFE is not aware about the external connection type.

Refer to the QorIQ LS1012A Reference Manual, 28.5.13 Protocol Configuration Register 8 (PCCR8):
"Field
SGMIIA_KX
SGMIIb 1000Base-KX Configuration:

Note: this configuration bit must be set before performing any MDIO initialization of the PCS.
0b - SGMII mode
1b - 1000Base-KX mode"

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,618件の閲覧回数
dolphin1
Contributor I

Ok. Thanks!

0 件の賞賛
返信
2,619件の閲覧回数
ufedor
NXP Employee
NXP Employee

Technically, direct MAC-to-MAC connection over SGMII is possible for the LS1012A.

The PFE is not aware about the external connection type.

Refer to the QorIQ LS1012A Reference Manual, 28.5.13 Protocol Configuration Register 8 (PCCR8):
"Field
SGMIIA_KX
SGMIIb 1000Base-KX Configuration:

Note: this configuration bit must be set before performing any MDIO initialization of the PCS.
0b - SGMII mode
1b - 1000Base-KX mode"

0 件の賞賛
返信