LS1012A MDIO Interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1012A MDIO Interface

2,111件の閲覧回数
rahulsoni
Contributor II

Hello NXP Team,

 

I'm designing a custom board based on LS1012A which has an ethernet switch IC and another ethernet PHY.

I have 3 MDIO interfaces in total while my processor supports only one MDIO interface.

 

I have read that an MDIO interface can manage up to 32 PHYs with different PHY addresses.

I want to confirm if MDIO driver of LS1012A can support the connection to more than 1 PHYs on MDIO interface?

Can I connect 3 MDIO interfaces of different PHYs to the MDIO interface on LS1012A?

 

Please confirm. 

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,868件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Can I connect 3 MDIO interfaces of different PHYs to the MDIO interface on LS1012A?

Yes, this is possible.

0 件の賞賛
返信