LS1012A MDIO Interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1012A MDIO Interface

2,101 Views
rahulsoni
Contributor II

Hello NXP Team,

 

I'm designing a custom board based on LS1012A which has an ethernet switch IC and another ethernet PHY.

I have 3 MDIO interfaces in total while my processor supports only one MDIO interface.

 

I have read that an MDIO interface can manage up to 32 PHYs with different PHY addresses.

I want to confirm if MDIO driver of LS1012A can support the connection to more than 1 PHYs on MDIO interface?

Can I connect 3 MDIO interfaces of different PHYs to the MDIO interface on LS1012A?

 

Please confirm. 

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,858 Views
ufedor
NXP Employee
NXP Employee

> Can I connect 3 MDIO interfaces of different PHYs to the MDIO interface on LS1012A?

Yes, this is possible.

0 Kudos
Reply