LS1012A LLDP booting issue.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1012A LLDP booting issue.

2,285件の閲覧回数
Gyosun
Contributor III

Hello,

I am using a custom board similar to ls1012afrwy.
I am porting the LLDP SDK(lf-6.1.1-1.0.0-langdale),
and uboot has been successfully ported to SPI Flash.
When trying to boot from the SD card in uboot, it stops at the next part and does not proceed.
Please advise.

...

[ 2.852721] BMU2 version: 21
[ 2.855630] EGPI1 version: 50
[ 2.858625] EGPI2 version: 50
[ 2.861627] HGPI version: 50
[ 2.864580] HIF version: 10
[ 2.867462] HIF NOPCY version: 10
[ 2.870875] bmu_init(1) done
[ 2.873849] bmu_init(2) done <-- stop fail!

This is the full boot log.

LLDP_ls1012afrwy_boot.log 

 

Thank you,
Best Regards.
Gyosun.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,025件の閲覧回数
Versenkt
Contributor II

Hello Gyosun,

I encountered the same problem. Have you found the reason?

0 件の賞賛
返信

1,981件の閲覧回数
Gyosun
Contributor III

Hi Versenkt,

Memories can become hazy as time passes.
I copied the ls1012afrwy_boot.scr (LSDK18.12), which used to boot well, into the boot folder and booted it.I hope this helps.

Have a good day.
Gyosun.

0 件の賞賛
返信

2,233件の閲覧回数
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

Please take a look on the LLDPUG:

The U-Boot based composite firmware must be programmed in flash device (not in SD card) on
LS2088ARDB/LS1012ARDB/LS1012AFRWY, no limitation on other Layerscape boards

0 件の賞賛
返信