LS1012A Kernel module for Ubuntu

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1012A Kernel module for Ubuntu

ソリューションへジャンプ
2,361件の閲覧回数
epoletaev
Contributor III

Hi,
I followed the LSDK manual to build a kernel and a my kernel module using Yocto layers.
Now I'm running Ubuntu root fs and cannot use my kernel module because at least it has a different kernel version.
How can I compile the Ubuntu kernel? Should I use LSDK? Can I use kernel compiled with Yocto?

0 件の賞賛
返信
1 解決策
2,294件の閲覧回数
June_Lu
NXP TechSupport
NXP TechSupport

Do you want install it into the storage device?

Please refer to LSDK21.08 4.3.8 How to generate LSDK bootpartition tarball.

4.3.13 How to build various userland with custom packages

LSDK Ubuntu-based Main Userland

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,295件の閲覧回数
June_Lu
NXP TechSupport
NXP TechSupport

Do you want install it into the storage device?

Please refer to LSDK21.08 4.3.8 How to generate LSDK bootpartition tarball.

4.3.13 How to build various userland with custom packages

LSDK Ubuntu-based Main Userland

0 件の賞賛
返信
2,318件の閲覧回数
June_Lu
NXP TechSupport
NXP TechSupport

Please refer to LSDK21.08 4.3.6 How to build Linux kernel with flex-builder.

0 件の賞賛
返信
2,313件の閲覧回数
epoletaev
Contributor III

Thanks @June_Lu , I already compiled the kernel. My question is how can I install it on Ubuntu?

0 件の賞賛
返信