LS1012A Boot from SD Card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1012A Boot from SD Card

ソリューションへジャンプ
2,499件の閲覧回数
igor_franco
Contributor IV

Hello,

I'm using the LS1012A Freeway board as an evaluation board. I noticed in the Getting Started Guide document that the board uses a QSPI to load the RCW. However, we desired to use only a MMC device. Is it possible to boot from SD Card or eMMC? Or the boot only can be performed by QSPI?

Thank you in advance,

Igor

0 件の賞賛
返信
1 解決策
2,492件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Is it possible to boot from SD Card or eMMC?

No - refer to the QorIQ LS1012A Reference Manual, Table 4-8. RCW source encodings.

> Or the boot only can be performed by QSPI?

Yes.

元の投稿で解決策を見る

2 返答(返信)
2,493件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Is it possible to boot from SD Card or eMMC?

No - refer to the QorIQ LS1012A Reference Manual, Table 4-8. RCW source encodings.

> Or the boot only can be performed by QSPI?

Yes.

2,490件の閲覧回数
igor_franco
Contributor IV

Hello, ufedor,

Thank you for your answer.

I will mark it as the solution.

Best regards,

Igor

0 件の賞賛
返信