LS1012A Boot from SD Card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1012A Boot from SD Card

Jump to solution
2,510 Views
igor_franco
Contributor IV

Hello,

I'm using the LS1012A Freeway board as an evaluation board. I noticed in the Getting Started Guide document that the board uses a QSPI to load the RCW. However, we desired to use only a MMC device. Is it possible to boot from SD Card or eMMC? Or the boot only can be performed by QSPI?

Thank you in advance,

Igor

0 Kudos
Reply
1 Solution
2,503 Views
ufedor
NXP Employee
NXP Employee

> Is it possible to boot from SD Card or eMMC?

No - refer to the QorIQ LS1012A Reference Manual, Table 4-8. RCW source encodings.

> Or the boot only can be performed by QSPI?

Yes.

View solution in original post

2 Replies
2,504 Views
ufedor
NXP Employee
NXP Employee

> Is it possible to boot from SD Card or eMMC?

No - refer to the QorIQ LS1012A Reference Manual, Table 4-8. RCW source encodings.

> Or the boot only can be performed by QSPI?

Yes.

2,501 Views
igor_franco
Contributor IV

Hello, ufedor,

Thank you for your answer.

I will mark it as the solution.

Best regards,

Igor

0 Kudos
Reply