LPUART on LS1046A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPUART on LS1046A

1,416 Views
matthej
Contributor II

Hi,

 

I have the LS1046ARDB eval board schematics which show the DUART connection to an RS232 xcvr and RJ45 connector.

 

I wanted to do the same thing for the LPUART on the LS1046A processor (connect it to the RS232 xcvr and then a connector.

0 Kudos
Reply
2 Replies

1,392 Views
matthej
Contributor II

Sorry, it appears that my question was cut off somehow.

 

So I wanted to connect the LPUART interface the same way as the DUART interface as on LS1046ARDB board (RS232 transceiver and then a connector).

 

Can this be done? I can't seem to find anything that shows how this interface is hooked up.

 

Thanks!

0 Kudos
Reply

1,410 Views
Pavel
NXP Employee
NXP Employee

The LS1046 LPUART is supported in LSDK 2012.

See the Table 4 in LSDK 2012 User Guide:

https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev20.12.pdf

 

Use the Section 7.2.7 in LSDK 2012 User Guide for LPUART setting on the LS1046a board.

0 Kudos
Reply