LLDP support in LS1028ARDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LLDP support in LS1028ARDB

3,991 Views
sameer_chouksey
Contributor II

Hello people,

I am trying to integrate the LS1028 board in a bigger network where I need LLDP service discovery protocol to be running the board. Does the LS1028 supports LLDP? Do we have some libraries available to enable it??

Thanks & Regards,

Sameer 

0 Kudos
Reply
4 Replies

3,886 Views
sameer_chouksey
Contributor II

Thanks for the responses. 

The LLDP package can be added using the menuconfig while building the OpenIL. After rebuilding the OpenIL with LLDP, it is working fine for me.

Regards,

Sameer 

0 Kudos
Reply

3,886 Views
yipingwang
NXP TechSupport
NXP TechSupport

The group in charge of LS1028A software doesn't do any LLDP specific testing.

That being said, there are no known problems surrounding it, since there is no special platform-level support required for LLDP.

In OpenIL 1.8, one can enable BR2_PACKAGE_LLDPD. For testing, the resulting rootfs can be deployed on 2 LS1028A-RDB boards, and a cable connecting eno0 to swp0 can be added.

The lldpd daemon is started automatically by /etc/init.d/S60lldpd. So, the lldpcli can be used directly:

Board 1:

[lldpcli] # show neighbors

-------------------------------------------------------------------------------

LLDP neighbors:

-------------------------------------------------------------------------------

Interface:    swp0, via: LLDP, RID: 1, Time: 0 day, 00:00:14

  Chassis:

    ChassisID:    mac 00:04:9f:05:f4:ab

    SysName:      LS1028ARDB

    SysDescr:     Buildroot 2020.02 Linux 5.4.3-rt1 #1 SMP PREEMPT_RT Thu Jun 18 20:20:05 EEST 2020 aarch64

    MgmtIP:       10.0.0.118

    MgmtIP:       fdc4:515b:d932:0:1911:3a70:8089:e509

    Capability:   Bridge, off

    Capability:   Router, off

    Capability:   Wlan, off

    Capability:   Station, on

  Port:

    PortID:       mac 00:04:9f:05:f4:ab

    PortDescr:    eno0

    TTL:          120

-------------------------------------------------------------------------------

Board 2:

[lldpcli] # show neighbors

-------------------------------------------------------------------------------

LLDP neighbors:

-------------------------------------------------------------------------------

Interface:    eno0, via: LLDP, RID: 1, Time: 0 day, 00:00:06

  Chassis:

    ChassisID:    mac 00:04:9f:05:de:06

    SysName:      LS1028ARDB

    SysDescr:     Buildroot 2020.02 Linux 5.4.3-rt1 #1 SMP PREEMPT_RT Thu Jun 18 20:20:05 EEST 2020 aarch64                                                                                                 

    MgmtIP:       10.0.0.112

    MgmtIP:       fdc4:515b:d932:0:7c7c:df93:5af5:b85

    Capability:   Bridge, off

    Capability:   Router, off

    Capability:   Wlan, off

    Capability:   Station, on

  Port:

    PortID:       mac 00:04:9f:05:de:0a

    PortDescr:    swp0

    TTL:          120

-------------------------------------------------------------------------------

 

So the 2 boards see each other.

 

It is not mandatory to use lldpd, this is just an example.

0 Kudos
Reply

3,886 Views
baiyu
Contributor I

Hi,Yiping

As you mentioned, "The lldpd daemon is started automatically by /etc/init.d/S60lldpd."

But i can't find S60lldpd in etc filefolder when trying to do LLDP.

0 Kudos
Reply

3,886 Views
baiyu
Contributor I
0 Kudos
Reply