Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b

2,726件の閲覧回数
fayeting
Contributor II

hi.

I am trying to compile the system for OK1046A-C2 board.

U-Boot version: U-Boot 2018.03
Kernel version: Linux 4.14

Compilation completed without any issues, but an error occurred during flashing with USB.

The printed information is as follows.

How can this problem be resolved?

Thanks!

 

タグ(1)
0 件の賞賛
返信
1 返信

2,713件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Something happens that the usb is disconnected and connected again in the midle of transfer data, I just try to burn again the BSP with the latest kernel to avoid this error.

Regards

0 件の賞賛
返信