Is there multiplexer/de-multiplexer for DPAA similar to dpdmux for DPAA2?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there multiplexer/de-multiplexer for DPAA similar to dpdmux for DPAA2?

ソリューションへジャンプ
808件の閲覧回数
FelixChang
Contributor I

As title, looking for the multiplexer/de-multiplexer method for DPAA platform. 
is there any keywords or advices to move forward on this topic? 

0 件の賞賛
返信
1 解決策
759件の閲覧回数
SebastianG
NXP TechSupport
NXP TechSupport

Hi @FelixChang,

Due to the LS1046ARDB use DPAA  as you can see in the following image

SebastianG_0-1683818121866.png

Also according to the DPAA manual "LS1046ADPAARM.pdf" and the DPAA2 manual this feature is only available in DPAA2

Regards,

Sebastian

元の投稿で解決策を見る

3 返答(返信)
781件の閲覧回数
FelixChang
Contributor I

Hi @SebastianG ,
thanks for your response.

I am working on ls1046 platform and traffic multiplexing/demultiplexing feature in DPAA.

we use 10G SFP (mac10) for data traffic,

boot fsl-ls1046a-rdb-usdpaa-shared-mac10.dtb 

fmc -x
fmc -c /usr/local/dpdk/dpaa/usdpaa_config_ls1046_shared_mac10.xml -p /usr/local/dpdk/dpaa/usdpaa_policy_vsp_classif_udp_ipsec_mac10_1queue.xml -a

but there are VSP assigment issues and result in mac10 init failed, any advices or document for me to refence ? 

mac10_initffail.png






0 件の賞賛
返信
760件の閲覧回数
SebastianG
NXP TechSupport
NXP TechSupport

Hi @FelixChang,

Due to the LS1046ARDB use DPAA  as you can see in the following image

SebastianG_0-1683818121866.png

Also according to the DPAA manual "LS1046ADPAARM.pdf" and the DPAA2 manual this feature is only available in DPAA2

Regards,

Sebastian

793件の閲覧回数
SebastianG
NXP TechSupport
NXP TechSupport

Hi @FelixChang,

I hope this post finds you well,

I would like to inform you that I keep working on your question

Regards,

Sebastian

0 件の賞賛
返信