Is there multiplexer/de-multiplexer for DPAA similar to dpdmux for DPAA2?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there multiplexer/de-multiplexer for DPAA similar to dpdmux for DPAA2?

Jump to solution
811 Views
FelixChang
Contributor I

As title, looking for the multiplexer/de-multiplexer method for DPAA platform. 
is there any keywords or advices to move forward on this topic? 

0 Kudos
Reply
1 Solution
762 Views
SebastianG
NXP TechSupport
NXP TechSupport

Hi @FelixChang,

Due to the LS1046ARDB use DPAA  as you can see in the following image

SebastianG_0-1683818121866.png

Also according to the DPAA manual "LS1046ADPAARM.pdf" and the DPAA2 manual this feature is only available in DPAA2

Regards,

Sebastian

View solution in original post

3 Replies
784 Views
FelixChang
Contributor I

Hi @SebastianG ,
thanks for your response.

I am working on ls1046 platform and traffic multiplexing/demultiplexing feature in DPAA.

we use 10G SFP (mac10) for data traffic,

boot fsl-ls1046a-rdb-usdpaa-shared-mac10.dtb 

fmc -x
fmc -c /usr/local/dpdk/dpaa/usdpaa_config_ls1046_shared_mac10.xml -p /usr/local/dpdk/dpaa/usdpaa_policy_vsp_classif_udp_ipsec_mac10_1queue.xml -a

but there are VSP assigment issues and result in mac10 init failed, any advices or document for me to refence ? 

mac10_initffail.png






0 Kudos
Reply
763 Views
SebastianG
NXP TechSupport
NXP TechSupport

Hi @FelixChang,

Due to the LS1046ARDB use DPAA  as you can see in the following image

SebastianG_0-1683818121866.png

Also according to the DPAA manual "LS1046ADPAARM.pdf" and the DPAA2 manual this feature is only available in DPAA2

Regards,

Sebastian

796 Views
SebastianG
NXP TechSupport
NXP TechSupport

Hi @FelixChang,

I hope this post finds you well,

I would like to inform you that I keep working on your question

Regards,

Sebastian

0 Kudos
Reply