As title, looking for the multiplexer/de-multiplexer method for DPAA platform.
is there any keywords or advices to move forward on this topic?
Solved! Go to Solution.
Hi @FelixChang,
Due to the LS1046ARDB use DPAA as you can see in the following image
Also according to the DPAA manual "LS1046ADPAARM.pdf" and the DPAA2 manual this feature is only available in DPAA2
Regards,
Sebastian
Hi @SebastianG ,
thanks for your response.
I am working on ls1046 platform and traffic multiplexing/demultiplexing feature in DPAA.
we use 10G SFP (mac10) for data traffic,
boot fsl-ls1046a-rdb-usdpaa-shared-mac10.dtb
fmc -x
fmc -c /usr/local/dpdk/dpaa/usdpaa_config_ls1046_shared_mac10.xml -p /usr/local/dpdk/dpaa/usdpaa_policy_vsp_classif_udp_ipsec_mac10_1queue.xml -a
but there are VSP assigment issues and result in mac10 init failed, any advices or document for me to refence ?
Hi @FelixChang,
Due to the LS1046ARDB use DPAA as you can see in the following image
Also according to the DPAA manual "LS1046ADPAARM.pdf" and the DPAA2 manual this feature is only available in DPAA2
Regards,
Sebastian
Hi @FelixChang,
I hope this post finds you well,
I would like to inform you that I keep working on your question
Regards,
Sebastian