Is the DPL content a device tree file?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is the DPL content a device tree file?

ソリューションへジャンプ
2,017件の閲覧回数
m_kei
Contributor III

I'm using LX2160ardb_rev2

Originally, there is no Ethernet driver for the LX2160 in linux, but when booting ubuntu from uboot, the Ethernet driver is enabled in ubuntu by sf reading the DPL file and then setting the boot configuration with fsl_mc.

I believe the entity of this DPL file is "dpl-eth.19.dtb", is this correct?

And if so, is it correct to recognize that DPL file = DTB file?

0 件の賞賛
返信
1 解決策
2,009件の閲覧回数
kenli
NXP Employee
NXP Employee

Yes, this is for configuring the mc. Note that both dpc adn dpl need to be configured correctly.

Best regards

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,010件の閲覧回数
kenli
NXP Employee
NXP Employee

Yes, this is for configuring the mc. Note that both dpc adn dpl need to be configured correctly.

Best regards
0 件の賞賛
返信