Is the DPL content a device tree file?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is the DPL content a device tree file?

Jump to solution
2,018 Views
m_kei
Contributor III

I'm using LX2160ardb_rev2

Originally, there is no Ethernet driver for the LX2160 in linux, but when booting ubuntu from uboot, the Ethernet driver is enabled in ubuntu by sf reading the DPL file and then setting the boot configuration with fsl_mc.

I believe the entity of this DPL file is "dpl-eth.19.dtb", is this correct?

And if so, is it correct to recognize that DPL file = DTB file?

0 Kudos
Reply
1 Solution
2,010 Views
kenli
NXP Employee
NXP Employee

Yes, this is for configuring the mc. Note that both dpc adn dpl need to be configured correctly.

Best regards

View solution in original post

0 Kudos
Reply
1 Reply
2,011 Views
kenli
NXP Employee
NXP Employee

Yes, this is for configuring the mc. Note that both dpc adn dpl need to be configured correctly.

Best regards
0 Kudos
Reply