Inclusive or exclusive caches model

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Inclusive or exclusive caches model

ソリューションへジャンプ
4,486件の閲覧回数
renatosala
Contributor I

Does the LS1043A use an exclusive caches model ? Is it possible to modify the this cache policy ?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,968件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

For data accesses, the Cortex-A53 uses "tends towards exclusive" cache allocation policy:

  "Data is allocated to the L2 cache only when evicted from the L1 memory system, not when first fetched from the system. The only exceptions to this rule are for memory marked with the inner transient hint, or for non-temporal loads, see Non-temporal loads, that are only ever allocated to the L2 cache. The L1 cache can prefetch data from the system, without data being evicted from the L2 cache."

 

For instruction fetches, the Cortex-A53 uses "tends towards inclusive" cache allocation policy:

   "Instructions are allocated to the L2 cache when fetched from the system and can be invalidated during maintenance

operations."

It is impossible to modify the this cache policy, this is non-configurable.

Please see

ARM Information Center 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
3,969件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

For data accesses, the Cortex-A53 uses "tends towards exclusive" cache allocation policy:

  "Data is allocated to the L2 cache only when evicted from the L1 memory system, not when first fetched from the system. The only exceptions to this rule are for memory marked with the inner transient hint, or for non-temporal loads, see Non-temporal loads, that are only ever allocated to the L2 cache. The L1 cache can prefetch data from the system, without data being evicted from the L2 cache."

 

For instruction fetches, the Cortex-A53 uses "tends towards inclusive" cache allocation policy:

   "Instructions are allocated to the L2 cache when fetched from the system and can be invalidated during maintenance

operations."

It is impossible to modify the this cache policy, this is non-configurable.

Please see

ARM Information Center 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------