ISR file for LS1021A?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ISR file for LS1021A?

1,494 Views
sukruthrameshba
Contributor III

Can you please provide the file containing the implementations of the generic interrupt
 controller handling routines for LS1021A?

Project is compiled and flash file is generated using code warrior.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,431 Views
Pavel
NXP Employee
NXP Employee

Look at program example in CodeWarrior folder. For example, use the following path to DUART program example:

C:\Freescale\CW4NET_v2016.01\CW_ARMv7\ARMv7\ARM_Support\Serial\Common

 

This example uses interrupt from DUART.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply