ISR file for LS1021A?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ISR file for LS1021A?

1,503 次查看
sukruthrameshba
Contributor III

Can you please provide the file containing the implementations of the generic interrupt
 controller handling routines for LS1021A?

Project is compiled and flash file is generated using code warrior.

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,440 次查看
Pavel
NXP Employee
NXP Employee

Look at program example in CodeWarrior folder. For example, use the following path to DUART program example:

C:\Freescale\CW4NET_v2016.01\CW_ARMv7\ARMv7\ARM_Support\Serial\Common

 

This example uses interrupt from DUART.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复