ISR file for LS1021A?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ISR file for LS1021A?

1,493件の閲覧回数
sukruthrameshba
Contributor III

Can you please provide the file containing the implementations of the generic interrupt
 controller handling routines for LS1021A?

Project is compiled and flash file is generated using code warrior.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,430件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at program example in CodeWarrior folder. For example, use the following path to DUART program example:

C:\Freescale\CW4NET_v2016.01\CW_ARMv7\ARMv7\ARM_Support\Serial\Common

 

This example uses interrupt from DUART.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信