How to use sd boot for ls1012ardb(or ls1012afrdm)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use sd boot for ls1012ardb(or ls1012afrdm)

1,557件の閲覧回数
mukunkong
Contributor I

With layerscape,I want deploy <firmware_ls1012ardb_uboot_qspiboot.img+bootpartition_arm64_lts_4.14.tgz+ubuntu userland> to ls1012ardb,but layserscape sdk document display ls1012ardb ony one boot method which is QSPI flash,

but if install <bootpartition_arm64_lts_4.14.tgz+ubuntu userland> to sd use qspi img to loading or not,someone help me?

0 件の賞賛
返信
1 返信

1,468件の閲覧回数
ufedor
NXP Employee
NXP Employee

By design the LS1012A is capable to boot from QSPI only - refer to the QorIQ LS1012A Reference Manual, 4.4.4.1 Reset configuration word (RCW) source.

This is why only QSPI booting is supported in the NXP LSDK.

0 件の賞賛
返信