Media type selection is purely a function of the PHY. Depending on the
PHY model, this can happen automatically or can be strap or software
configured. Consult at your PHY documentation/manufacturer. If it is
software-configurable for your PHY, the PHY driver may read additional
properties from the Device Tree, however, they are not standard and
fully depend on the driver. Again, the suggestion is to study the
driver code or contact it's maintainer for additional information.
Have a great day,
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------