Hello everyone,
I would like to create the file "firmware_ls1043ardb_sdboot.img" which must be loaded on the SD card using a RCW modified by me.
Flex-builder works with a lot of files (RCW, U-boot,...), different for each board and compiles them all together based on the type of command launched.
The command that allows me to compile all the files for a specific board and get the ".img " is the following:
"$flex-builer -i mkfw -m ls1043ardb -b sd"
But I want to change RCW, change the working frequency and disable core (core 1, core 2, core 3 ) of the processor.
From what I seem to have understood every time I run the command, it goes to check the file
<flexbuild> / configs / board / <machine> / manifest
An excerpt from the first part of manifest:
machine="ls1043ardb"
# default RCW
rcw_nor="firmware/rcw/ls1043ardb/RR_FQPP_1455/rcw_1600.bin"
rcw_nor_sec="firmware/rcw/ls1043ardb/RR_FQPP_1455/rcw_1600_sben.bin"
rcw_sd="firmware/rcw/ls1043ardb/RR_FQPP_1455/rcw_1600_sdboot.bin"
rcw_sd_sec="firmware/rcw/ls1043ardb/RR_FQPP_1455/rcw_1600_sdboot_sben.bin"
rcw_nand="firmware/rcw/ls1043ardb/RR_FQPP_1455/rcw_1600_nandboot.bin"
rcw_nand_sec="firmware/rcw/ls1043ardb/RR_FQPP_1455/rcw_1600_nandboot_sben.bin"
uefi_nor="firmware/uefi/ls1043ardb/LS1043ARDB_EFI_NORBOOT.fd"
device_tree="linux/kernel/arm64/LS/fsl-ls1043a-rdb-sdk.dtb"
BOOT_TYPE="sd nor nand"
BOOTLOADER_TYPE="uboot uefi"
UBOOT_CONFIG="ls1043ardb_tfa_defconfig ls1043ardb_tfa_SECURE_BOOT_defconfig"
# RCW/PBL+BL2 image
COMPOSITE_IMG1_FILE_sd="firmware/atf/ls1043ardb/bl2_sd.pbl"
COMPOSITE_IMG1_FILE_sd_sec="firmware/atf/ls1043ardb/bl2_sd_sec.pbl"
COMPOSITE_IMG1_FILE_nor="firmware/atf/ls1043ardb/bl2_nor.pbl"
COMPOSITE_IMG1_FILE_nor_sec="firmware/atf/ls1043ardb/bl2_nor_sec.pbl"
COMPOSITE_IMG1_FILE_nand="firmware/atf/ls1043ardb/bl2_nand.pbl"
# BL33 fip image
COMPOSITE_IMG2_FILE="firmware/atf/ls1043ardb/fip_uboot.bin"
COMPOSITE_IMG2_FILE_sec="firmware/atf/ls1043ardb/fip_uboot_sec.bin"
COMPOSITE_IMG2_FILE_uefi="firmware/atf/ls1043ardb/fip_uefi.bin"
# bootloader UEFI environment variable
COMPOSITE_IMG3_FILE_uefi="firmware/uefi/ls1043ardb/LS1043ARDBNV_EFI_NORBOOT.fd"
I have to change this line rcw_sd="firmware/rcw/ls1043ardb/RR_FQPP_1455/rcw_1600_sdboot.bin" to rcw_sd="firmware/rcw/ls1043ardb/RR_FQPP_1455/rcw_1200_sdboot.bin" to run the board at 1.2GHz.
Not only that, inside the file rcw_1200_sdboot.bin I have to go write:
.pbi
write 0x01ee0094, 0x0000000e
.ebd
to disable cores.
the file rcw_1200_sdboot.bin is in this path:
flexbuild_lsdk2108/components/firmware/rcw/ls1043ardb/RR_FQPP_1455/rcw_1200_sdboot.bin
Once the RCW file has been modified, rerun the command $ flex-builer -i mkfw -m ls1043ardb -b sd and wait for the .img file to be generated.
Finally I insert the SD card formatted in Fat16 format
and I run the following command to load the file on the sd card:
sudo dd if=firmware_lx2160ardb_rev2_uboot_sdboot.img of=/dev/sdb bs=512 seek=8
Are the steps described up to here correct?
已解决! 转到解答。
Hi, thanks for your reply.
Although the procedure seems right, I am having problems.
I get nothing at all (via USB console), I don't see U-Boot.
I'm doing the steps in the most standard way without editing any files. I want to get an .img file capable of starting u-boot on my ls1043a platform.
So I download flex-builder from your site:www.nxp.com/lsdk.
I perform the following steps:
$ tar xvzf flexbuild_<version>.tgz
$ cd flexbuild_<verison>
$ source setup.env
$ flex-builder -h
After that I run the command:
$ flex-builder -i mkfw -m ls1043ardb -b sd
Which after a while gives me the following outputs:
firmware_ls1043ardb_sdboot.img
firmware_ls1043ardb_sdboot_secure.img
linux_LS_arm64_signature.itb
lsdk2108_yocto_tiny_LS_arm64.itb
rootfs_lsdk2108_yocto_tiny_arm64.cpio.gz
I'm only interested in: firmware_ls1043ardb_sdboot.img
I'm going to save the .img file in SD using the following command:
sudo dd if=firmware_ls1043ardb_sdboot.img of=/dev/sdb1 bs=512 seek=8
I use a USB adapter to insert SD card into my PC. I am running Ubuntu 20.04 through a virtual machine.
The writing seems to have been successful.
But when I try to boot from SD (set de DIP switches for SD boot), I don't see anything on the console.
I don't see Uboot starting.
I cannot understand where I am wrong. Having not changed anything, uboot should start without problems.