Hi All,
I'm using LS2085A QDS board and im facing errors like the following. The boot log is as followa
U-Boot 2015.07-rc1Layerscape2-SDK+g7e8bad0 (Oct 08 2015 - 20:08:11)
SoC: LS2085E (0x87010010)
Clock Configuration:
CPU0(A57):1600 MHz CPU1(A57):1600 MHz CPU2(A57):1600 MHz
CPU3(A57):1600 MHz CPU4(A57):1600 MHz CPU5(A57):1600 MHz
CPU6(A57):1600 MHz CPU7(A57):1600 MHz
Bus: 600 MHz DDR: 1333.333 MT/s DP-DDR: 1333.333 MT/s
Reset Configuration Word (RCW):
00: 40282830 40400040 00000000 00000000
10: 00000000 00200000 00200000 00000000
20: 01812980 00002580 00000000 00000000
30: 00000e0b 00000000 00000000 00000000
40: 00000000 00000000 00000000 00000000
50: 00000000 00000000 00000000 00000000
60: 00000000 00000000 00027000 00000000
70: 3f350000 00000000 00000000 00000000
Model: Freescale Layerscape 2085a QDS Board
Board: LS2085E-QDS, Board Arch: V1, Board version: B, boot from vBank: 0
FPGA: v5 (LS2085AQDS_2015_0218_1606), build 132 on Wed Feb 18 22:06:38 2015
SERDES1 Reference : Clock1 = 156.25MHz Clock2 = 100 separate SSCGMHz
SERDES2 Reference : Clock1 = 100 separate SSCGMHz Clock2 = 100 separate SSCGMHz
I2C: ready
DRAM: Initializing DDR....using SPD
Detected UDIMM 18ASF1G72AZ-2G1A1
Detected UDIMM 18ASF1G72AZ-2G1A1
Controler 0 timeout, debug_2 = 2100
Controler 0 timeout, debug_2 = 2500
Waiting for D_INIT timeout. Memory may not work.
Controler 1 timeout, debug_2 = 100
Controler 1 timeout, debug_2 = 1500
Waiting for D_INIT timeout. Memory may not work.
DP-DDR: Detected UDIMM 18ASF1G72AZ-2G1A1
The errors are indicated in red color, please help me to fix this issue.
Note: I didnt change any DDR related files, all the default images are already loaded in the board..
 yipingwang
		
			yipingwang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Anandha Kumar,
It seems that you customized the RCW file based on the default one, Can you boot up the board successfully with the default RCW file? If the problem also exists, would you please provide the switch configuration on your target board?
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
 
					
				
		
Hi Yiping,
I'm using the default RCW file only, also all the switch settings are proper and verified as per the user guide from Freescale document. I guess this might be due to frequency mismatch and some DDR issue with the board. Please comment on the same. Thanks for your valuable reply.
 yipingwang
		
			yipingwang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Anandha Kumar,
It looks that you used the u-boot image built from 20150828, but RCW is not from this release.
I built RCW and u-boot for LS2085AQDS with Layerscape2-SDK-20150828, please refer to the attachment.
Please try whether these images could work on your target board.
You could program these images to NOR flash from other bank if possible, or use CodeWarrior to do flash programming.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
 
					
				
		
Hi Yiping,
I flashed above images using Codewarrior flash programmer. Since the problem remains same.
Boot log:
===========
U-Boot 2015.07-rc1Layerscape2-SDK+g7e8bad0 (Jan 05 2016 - 15:43:31)
SoC: LS2085E (0x87010010)
Clock Configuration:
CPU0(A57):1600 MHz CPU1(A57):1600 MHz CPU2(A57):1600 MHz
CPU3(A57):1600 MHz CPU4(A57):1600 MHz CPU5(A57):1600 MHz
CPU6(A57):1600 MHz CPU7(A57):1600 MHz
Bus: 600 MHz DDR: 1333.333 MT/s DP-DDR: 1333.333 MT/s
Reset Configuration Word (RCW):
00: 40282830 40400040 00000000 00000000
10: 00000000 00200000 00200000 00000000
20: 00c12980 00002580 00000000 00000000
30: 00000e0b 00000000 00000000 00000000
40: 00000000 00000000 00000000 00000000
50: 00000000 00000000 00000000 00000000
60: 00000000 00000000 00027000 00000000
70: 492a0000 00000000 00000000 00000000
Model: Freescale Layerscape 2085a QDS Board
Board: LS2085E-QDS, Board Arch: V1, Board version: B, boot from vBank: 4
FPGA: v5 (LS2085AQDS_2015_0218_1606), build 132 on Wed Feb 18 22:06:38 2015
SERDES1 Reference : Clock1 = 156.25MHz Clock2 = 100MHz
SERDES2 Reference : Clock1 = 100MHz Clock2 = 100MHz
I2C: ready
DRAM: Initializing DDR....using SPD
Detected UDIMM 18ASF1G72AZ-2G1A1
Detected UDIMM 18ASF1G72AZ-2G1A1
Controler 0 timeout, debug_2 = 2100
Controler 0 timeout, debug_2 = 2500
Waiting for D_INIT timeout. Memory may not work.
Controler 1 timeout, debug_2 = 2100
Controler 1 timeout, debug_2 = 2500
Waiting for D_INIT timeout. Memory may not work.
DP-DDR: Detected UDIMM 18ASF1G72AZ-2G1A1
=============
May i know why this issue is occurred and how to solve it?
Thanks for your great responses,
Thanks Regards,
-Anandha Kumar
Hi all,
Can anyone help me on, to fix this issue?
Thanks,
-Naveen
 yipingwang
		
			yipingwang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Naveen,
It seems that you have used this LS2085AQDS board for several months, why did you encounter this problem suddenly? I am not sure what modification you have done, I suspect you updated to the new version u-boot recently, and this u-boot is not compatible with the FPGA firmware on your target, We use FPGA v7 on the board farm board.
So I suggest you program old version u-boot back and check whether this problem remains, if it disappears, you could consider about updating to new version FPGA.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yiping,
From Starting itself we are using EAR4 images. Recently we changed to EAR5 images, for that also its working fine for a while.
Now we are facing this boot error issue. I flashed default EAR4 images via JTAG programmer.
But still the problem remains same.
What's the solution for that?
Thanks,
-Naveen
 yipingwang
		
			yipingwang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Naveen,
Please use CodeWarrior to debug a sample program in DDR memory to check whether the program could be executed successfully in DDR.
Thanks,
Yiping
 ed_swarthout
		
			ed_swarthout
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Is the processor on this board in a socket? If so, can you re-seat the processor to see if this is a mechanical issue?
Hi,
For me still the issue remains same.
Is there any other way to fix this issue?
Thanks,
-Naveen