How to resolve Synchronous Abort handler issue for PCIe PEX4?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to resolve Synchronous Abort handler issue for PCIe PEX4?

2,727件の閲覧回数
meenachik
Contributor I

Hi all,

The PCIe PEX4 bus enumeration problem for LS2088A board.I have Configured PEX2/PEX4 as RC and PEX3 as EP.
The PEX2 is configured as RC & PEX3 as EP while booting.The PEX4 bus enumeration produces the Synchronous Abort issue.

U-Boot Log:

U-Boot 2016.01LS2088A-SDK+g8870d3a (Aug 01 2017 - 20:31:06 +0530)

SoC: LS2088E Version:1.0 (0x87090010)
Clock Configuration:
CPU0(A72):1600 MHz CPU1(A72):1600 MHz CPU2(A72):1600 MHz
CPU3(A72):1600 MHz CPU4(A72):1600 MHz CPU5(A72):1600 MHz
CPU6(A72):1600 MHz CPU7(A72):1600 MHz
Bus: 600 MHz DDR: 1333.333 MT/s DP-DDR: 1333.333 MT/s
Reset Configuration Word (RCW):
00000000: 40282830 40400040 00000000 00000000
00000010: 00000000 00000000 00200000 00000000
00000020: 0b212980 00002580 00000000 00000000
00000030: 00000a08 00000000 00000000 00000080
00000040: 00000000 00000000 00000000 00000000
00000050: 00000000 00000000 00000000 00000000
00000060: 00000000 00000000 00027000 00000000
00000070: 51350000 00000000 00000000 00000000
I2C: ready
Model: Freescale Layerscape 2088a ISSD Board
Board: LS2085A/LS2088A-QDS, Board Arch: V1, Board Version: A
CPLD_NIC Version: A10
DRAM: Initializing DDR....using SPD
Detected UDIMM 9965657-004.A00G
Detected UDIMM 9965657-004.A00G
Address hashing enabled.
Address hashing enabled.
15 GiB
DDR 15 GiB (DDR4, 64-bit, CL=9, ECC on)
DDR Controller Interleaving Mode: 256B
DDR Chip-Select Interleaving Mode: CS0+CS1
fsl-ppa: Bad firmware image (not a FIT image)
fsl-ppa: error (-22)
fsl-ppa: Bad firmware image (not a FIT image)
Waking secondary cores to start from fff14000
All (8) cores are up.
Using SERDES1 Protocol: 53 (0x35)
Using SERDES2 Protocol: 81 (0x51)
Flash: 128 MiB
MMC: FSL_SDHC: 0
EEPROM: NXID v1
PCIe1: disabled
PCIe2: Root Complex x4 gen2, regs @ 0x3500000
PCI:
01:00.0 - 1957:0953 - Mass storage controller

PCIe2: Bus 00 - 01
PCIe3: Endpoint x4 gen1, regs @ 0x3600000
PCIe4: Root Complex x4 gen2, regs @ 0x3700000
PCI:
"Synchronous Abort" handler, esr 0x96000005
ELR: fff56300
LR: fff56278
x0 : 0000003800000000 x1 : 0000000001000000
x2 : 000000380000000c x3 : 0000000000000003
x4 : 0000000000000003 x5 : 0000000000000000
x6 : 0000000000000000 x7 : 0000000000000000
x8 : 0000000000000190 x9 : 000000000000000c
x10: 00000000000003ff x11: 0000000000000000
x12: 0000000000000001 x13: 0000000040000000
x14: 0000000000200000 x15: 0000000000000001
x16: 0000000000000000 x17: 0000000000000000
x18: 00000000ffd0fd88 x19: 000000000000000c
x20: 00000000ffd10a40 x21: 0000000000000003
x22: 0000000000030000 x23: 00000000ffd0e1ec
x24: 00000000fff88da6 x25: 000000000003ff00
x26: 00000000fffbbc90 x27: 00000000fff89200
x28: 0000000000000000 x29: 00000000ffd0e180

Resetting CPU ...

### ERROR ### Please RESET the board ###

I have tried to trace the issue in u-boot source code

Workaround:
1. When pci_bus scannning process in u-boot,it tries to read the pcie_header_type abort occur.

PEX2 also configured as RC but it get bus enumeration correctly and PEX4 only arise this issue.

2. Disble the pcie_setup_ctrl in RC u-boot. PEX4 abort not arise.but PCIe both bus gets enumerated wrongly.In kernel ,PCI rescan is required to detected the device.

I do know the exact reason for this issue.If any one know about this.Please,help me to resolve this issue.


Thanks,
Meenachi

ラベル(1)
0 件の賞賛
返信
0 返答(返信)