How to make TSEC worked in LX2160

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to make TSEC worked in LX2160

ソリューションへジャンプ
2,786件の閲覧回数
howardlu1
Contributor I


Hi, All:

 

I already modified EC2 in RCW to make TSEC_1588 worked, but  when I input either 10MHZ or 125 MHZ to TSEC_1588_CLK_IN pin, and observe TSEC_1588_PULSE_OUT2 and 1588_PULSE_OUT1 both pins, they have signal but seems not synced from TSEC_1588_CLK_IN.

And 1588_ALARM_OUT1 have no signal out also. 

If I want PULSE_OUT1 or PULSE_OUT2 is synced from TSEC_1588_CLK_IN, is any other setting that need to be modified?

 

Thanks,

Howard.

0 件の賞賛
返信
1 解決策
2,762件の閲覧回数
r8070z
NXP Employee
NXP Employee

It is not clear how you program the LX2160A TSEC 1588 Timer Module. You can set PULSE_OUT1 or PULSE_OUT2 phased aligned to the prescale output clock (TSEC_1588_CLK_OUT). Please see details in the chapter “Timer Fixed Interval Period Register (TMR_FIPER1–3)” of the LX2160A DPAA2 Low-Level Hardware Reference Manual. It is available on the nxp LX2160 webpage. You also can set TSEC_1588_CLK_OUT as integer multiple value of TSEC_1588_CLK_IN (again see the chapter 1588 Timer IP Module in the DPAA2 manual). Hence you can get PULSE_OUT1 or PULSE_OUT2 synced from TSEC_1588_CLK_IN.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,763件の閲覧回数
r8070z
NXP Employee
NXP Employee

It is not clear how you program the LX2160A TSEC 1588 Timer Module. You can set PULSE_OUT1 or PULSE_OUT2 phased aligned to the prescale output clock (TSEC_1588_CLK_OUT). Please see details in the chapter “Timer Fixed Interval Period Register (TMR_FIPER1–3)” of the LX2160A DPAA2 Low-Level Hardware Reference Manual. It is available on the nxp LX2160 webpage. You also can set TSEC_1588_CLK_OUT as integer multiple value of TSEC_1588_CLK_IN (again see the chapter 1588 Timer IP Module in the DPAA2 manual). Hence you can get PULSE_OUT1 or PULSE_OUT2 synced from TSEC_1588_CLK_IN.

0 件の賞賛
返信