How to interface an external DUART chip with the ifc bus of an ls1021a-twr board?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to interface an external DUART chip with the ifc bus of an ls1021a-twr board?

2,129 次查看
sujay1
Contributor V

Hi,

I'm trying to interface an external duart XR68M752IM48  to my custom ls1021a-twr board's ifc bus,

 

Can you please tell me what are the changes I may have to make to the driver to interface this chip and also the changes I have to make in the dts file fot configure a duart node?

0 项奖励
回复
3 回复数

2,110 次查看
Pavel
NXP Employee
NXP Employee

See as example the AN12098:

https://www.nxp.com/webapp/Download?colCode=AN12098&location=null

 

It looks like the driver is needed the XR68M752IM48 using as duart on the LS1021a board.

The LS1021a supports 6 LPUARTs. Usually these UART are used if additional UARTs are needed.

 

Have a great day,
Pavel Chubakov

0 项奖励
回复

2,108 次查看
sujay1
Contributor V

Hi Pavel,

Is there any driver already available for this? also can you please explain in detail how to configure the kernel to add support for XR68M752IM48 .

0 项奖励
回复