How to implement xen-hypervisor in yocto? (LX2160A)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to implement xen-hypervisor in yocto? (LX2160A)

623 Views
peter_kang
Contributor I

How to implement xen-hypervisor in yocto? (LX2160A)

 

Hi,

We have built the SDK using the Yocto environment (Scarthgap branch) following the NXP repository:
https://github.com/nxp-qoriq/yocto-sdk

After deploying the images to an SD card, we successfully booted the reference board using the guidance provided here:
https://community.nxp.com/t5/Layerscape/LX2160-yocto-implement-problem/m-p/1367714

We are now working on integrating the Xen hypervisor.
To do so, we referred to the following legacy document:
https://www.nxp.com/docs/en/application-note/AN13138.pdf

We have successfully enabled Xen in the Yocto SDK build, based on the instructions in that document.

 

However, the document does not explain how to deploy the Xen-enabled image via SD card.

Could you please provide guidance on how to deploy the Yocto SDK with Xen support using an SD card?
Alternatively, if there is a better method for deployment, we would appreciate your recommendation.

Thank you.

Tags (3)
0 Kudos
Reply
1 Reply

590 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please connect SD card to your host PC

  1. Please create two partitions with Linux command "fdisk", one 1G FAT16 and 2G one ext2/ext3 or with remainder of the available disk size.
    # mkfs.vfat /dev/sdb1
    # mkfs.ext2 /dev/sdb2
    2. Please deploy rootfs filesystem to SD card in the host PC as the following.
    # mkdir  /temp
    # mount  /dev/sdb2  /temp
    # cd /temp
    # cp  fsl-image-networking-lx2160ardb.tar.gz .
    # tar -xzvf  fsl-image-networking-lx2160ardb.tar.gz
    # rm  fsl-image-networking-lx2160ardb.tar.gz
    Please deploy Kernel Image and the dtb to the /boot folder.
    # cp Image boot
    # cp  fsl-lx2160-rdb-sdk.dtb boot

    Configure the switch setting boot from SD card 

Plug in the SD card to the target board and power on.
Set the environment in uboot for SD boot.

=>
=> setenv bootcmd 'setenv bootargs root=/dev/mmcblk0p2 rw rootdelay=5 console=ttyAMA0,115200 earlycon=pl011,mmio32,0x21c0000;mmcinfo;mmc read 0x80d00000 0x6800 0x800; fsl_mc lazyapply dpl 0x80d00000;ext2load mmc 0:2 0xa0000000 /boot/Image;ext2load mmc 0:2 0xb0000000 /boot/fsl-lx2160a-rdb-sdk.dtb;booti 0xa0000000 - 0xb0000000'
=> saveenv

0 Kudos
Reply