How to generate RFS JFFS2 image or initramfs via flex-builder?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to generate RFS JFFS2 image or initramfs via flex-builder?

ソリューションへジャンプ
2,087件の閲覧回数
alance
Contributor II

Hi

Is it possible to build RFS with flex-builder and generate the JFFS2 image?

Or to build RFS to initramfs via flex-builder?

Thanks.

ラベル(2)
0 件の賞賛
返信
1 解決策
2,068件の閲覧回数
bpe
NXP Employee
NXP Employee

This is supported only for buildroot root filesystems. You can instruct flex-builder to create a buildroot rootfs by specifying -r option:

 

bpe_1-1600748384498.png


and configuring the options in the corresponding file under configs/buildroot/ as appropriate:

bpe_0-1600748133442.png

More details can be found in docs/flexbuild_usage.txt

 

Hope this helps

Platon

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,069件の閲覧回数
bpe
NXP Employee
NXP Employee

This is supported only for buildroot root filesystems. You can instruct flex-builder to create a buildroot rootfs by specifying -r option:

 

bpe_1-1600748384498.png


and configuring the options in the corresponding file under configs/buildroot/ as appropriate:

bpe_0-1600748133442.png

More details can be found in docs/flexbuild_usage.txt

 

Hope this helps

Platon

 

 

0 件の賞賛
返信