How to enable error injection on LS1043A DCache

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable error injection on LS1043A DCache

1,403 Views
aross
Contributor I

I am trying to test error handling for DCache ECC errors in bare-metal (running at EL3) on a LS1043ARDB.

If I set CPUACTLR_EL1.L1DEIEN (bit[6]) and then write a cacheable location, nothing seems to happen.

The CPUMESSR doesn't change, nor is there an abort, etc.

I have also tried L2 (L2ACTLR[29]) and caused an eviction from L1.

I can see the data is in the cache by reading the cache RAM.

I feel like I am missing some other enable somewhere?

Labels (1)
0 Kudos
Reply
2 Replies

1,365 Views
ufedor
NXP Employee
NXP Employee

You need to explicitly read(via LDR instruction) that cacheline again after the error is injected into corresponding caches(triggered by the previous write). CPUMERRSR or L2MERRSR can record the error information once the injected error line is read again.

0 Kudos
Reply

1,365 Views
aross
Contributor I

I looked closer at the data via reading the cache RAM and noticed it looks like it did flip 2 bits in the data. 

But didn't report any error. So maybe there's an enable for the cache ECC?

0 Kudos
Reply