How to create a new Qoriq Configuration Project for LS1024A in CodeWarrior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to create a new Qoriq Configuration Project for LS1024A in CodeWarrior

2,507 次查看
pmccormick
Contributor II

Hello, I am using Code Warrior / QCVS and I am trying to create a new Qoriq Configuration Project for use with the ddr test tool.  On the dialog box entitled "New Qoriq Configuration Project" I am being asked to "Select the processor you would like use" but LS1024A is not one of the choices, I only see LS1020A, LS1021A and LS1022A.  I am using "CodeWarrior Development Studio for QorIQ LS series - ARM V7 ISA Version: 10.0.9 Build Id:170914"  Am I perhaps missing some additional processor support files?  Is there some additional component I need to install?    With the same CodeWarrior install I have successfully used the debugger with the LS1024A, downloaded and stepped through code, programmed flash, etc.

标签 (1)
0 项奖励
回复
3 回复数

2,290 次查看
ufedor
NXP Employee
NXP Employee

LS1024A is not supported by the QCVS.

0 项奖励
回复

2,290 次查看
pmccormick
Contributor II

OK, so is there any plan to support LS1024A in a future version of QCVS?  Or a different nxp product I should be using instead?  I just want to run the ddr test tool...

0 项奖励
回复

2,290 次查看
ufedor
NXP Employee
NXP Employee

Sorry, no plans and no other tool.

0 项奖励
回复