How to check SEC_MON status in Linux ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to check SEC_MON status in Linux ?

跳至解决方案
1,225 次查看
Jeffrey_Lai
Contributor II

Hi,

We want to check LX2160ARDB security monitor (SEC_MON) status in Linux. 

According to LX2160A reference manual, we try to read SecMon address (0x1E9_0000) by devmem2 command as below but get the same value (0x0) at secure and non-secure mode.

root@localhost:~# devmem2 0x01e90000
/dev/mem opened.
Memory mapped at address 0xffff8aba8000.
Value at address 0x1E90000 (0xffff8aba8000): 0x0

Is it correct?

How to check SEC_MON status in Linux ?

 

Thank you,

Jeffrey

0 项奖励
回复
1 解答
1,212 次查看
yipingwang
NXP TechSupport
NXP TechSupport

The recent released LSDK comply with AT-F(ARM Trusted Firmware), so secure fuse is reading on EL3. Since Linux is running on EL2 and EL1, it does not have read access.

A option for you is to use JTAG(CCS+CodeWarrior TAP).

You could use the following CCS commands

% delete all

% config cc cwtap

% ccs::config_chain {lx2160a dap}

% display ccs::get_config_chain

% disp ccs::read_mem 86 0x1e90010 4 0 16                   

+0       +4       +8       +C 

[0x01E90010] 00000000 88002B00 80000000 00000000 

[0x01E90020] 00000000 00000000 00000000 00000000 

[0x01E90030] 00000000 00000000 00000000 00000000 

[0x01E90040] 00000000 00000000 00000000 00000008   

Note "86" above is chain position for SAP2 on my LX2160ARDB board

在原帖中查看解决方案

1 回复
1,213 次查看
yipingwang
NXP TechSupport
NXP TechSupport

The recent released LSDK comply with AT-F(ARM Trusted Firmware), so secure fuse is reading on EL3. Since Linux is running on EL2 and EL1, it does not have read access.

A option for you is to use JTAG(CCS+CodeWarrior TAP).

You could use the following CCS commands

% delete all

% config cc cwtap

% ccs::config_chain {lx2160a dap}

% display ccs::get_config_chain

% disp ccs::read_mem 86 0x1e90010 4 0 16                   

+0       +4       +8       +C 

[0x01E90010] 00000000 88002B00 80000000 00000000 

[0x01E90020] 00000000 00000000 00000000 00000000 

[0x01E90030] 00000000 00000000 00000000 00000000 

[0x01E90040] 00000000 00000000 00000000 00000008   

Note "86" above is chain position for SAP2 on my LX2160ARDB board