How to build a LS1017A processor project using CodeWarrior for ARM v8 2020.06

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to build a LS1017A processor project using CodeWarrior for ARM v8 2020.06

1,151 次查看
letisl
Contributor I

Hello, I am using the LS1017A processor and the CodeWarrior for ARM v8 2020.06 (CW ARM) software, but when I need to create a new BareBoard project, I find that there is no such option in CW ARM, as shown in the following figure:

letisl_2-1742780779826.pngletisl_2-1742780779826.png

 

In CodeWarrior for PowerPC 10.5.1 (CW PA), you can create a new BareBoard project:

letisl_1-1742780737369.pngletisl_1-1742780737369.png

 

Q1: How can I create a new BareBoard project to flash U-boot onto a new board?

 

There is another important issue, in CW ARM, it is not possible to select the LS1017 processor; only the following processor list is available:

letisl_3-1742780856238.pngletisl_3-1742780856238.png

 

Q2: How should I choose when using the LS1017A processor?

 

I'm looking for your help!

0 项奖励
回复
1 回复

1,090 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to section “3.2 Working with bareboard application” in C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\Help\Getting_Started_for_CW_ARMv8.pdf to create a bareboard project in CodeWarrior for ARMv8.

For flash programming, please refer to section "8.6 Board Recovery" in C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\Help\PDF\ARMv8_Targeting_Manual.pdf

0 项奖励
回复