How to access SRAM connected on IFC Bus?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to access SRAM connected on IFC Bus?

1,475 Views
winstonjacob
Contributor IV

Hi,

We are having a custom board with LS1021A-TWR processor. SRAM is connected on IFC bus with chip select 2. We need to access SRAM through MTD.

For this I have made some changes in dts as shown below.

&ifc {
#address-cells = <2>;
#size-cells = <1>;
/* NOR Flash on board and SRAM */
ranges = <0x0 0x0 0x0 0x60000000 0x08000000>
<0x2 0x0 0x0 0x7e800000 0x00080000>;
status = "okay";

nor@0,0 {

....

};

sram@2,0 {
compatible = "mtd-ram";
reg = <0x2 0x0 0x80000>;
bank-width = <2>;
};
/*
cpld@2,0 {
compatible = "fsl,ls1021atwr-cpld";
reg = <0x2 0x0 0x100>;
};
*/
};

The driver for the SRAM chip registers the device as a MTD.

~# cat /proc/mtd
dev: size erasesize name
mtd0: 00080000 00001000 "7e800000.sram"

But use of echo > and cat to the mtdblock results garbage.

Is there any changes required in kernel and u-boot side?

Labels (1)
0 Kudos
Reply
3 Replies

1,452 Views
Pavel
NXP Employee
NXP Employee

Is there problem for accessing to this SRAM under u-boot?

Test SRAM reading/writing under u-boot.

0 Kudos
Reply

1,447 Views
winstonjacob
Contributor IV

Not able to access SRAM under uboot. We don't have a clock in SRAM(IS62WV25616EBLL). In this case how to calculate the flash timing register values(need to configure in ls1021atwr.h file)?

0 Kudos
Reply

1,414 Views
Pavel
NXP Employee
NXP Employee

See the Section 24.3.11 in the LS1021a Reference Manual:

https://www.nxp.com/webapp/Download?colCode=LS1021ARM

 

See also the Table 76 in the LS1021a Datasheet:

https://www.nxp.com/webapp/Download?colCode=LS1021A

0 Kudos
Reply