How do I modify the LS1012A QSPI flash memory layout?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I modify the LS1012A QSPI flash memory layout?

1,978件の閲覧回数
timhammer
Contributor III

Is there any way to modify the placement of the U-Boot binary, U-Boot environment, and PPA FIT image in the QSPI? If we will never need the currently allocated amount of space for each item, I could shift everything down and have more memory for a small kernel/dtb/rootfs image, or use a smaller QSPI flash part.
I have looked through the PBL configuration documents I have found, but I do not see anything that indicates it is possible.

The PBI data used to create the PBL image does have a file uboot_address.rcw with commands to write some values:


write 0x570604, 0x40100000
write 0x57015c, 0x50100000
write 0x570600, 0x00000000

 

Based on the file name, I thought it might be what I was looking for, but the values do not make sense with either layout I have seen. Nor do the addresses to which the values are witten make much sense- according to the LS1012A reference manual (assuming these addresses are in the SCFG memory map), address 0x604 and 0x600 are in the scratch read/write registers, and 0x15c is the register for the QSPI clock source/enable/disable. Perhaps the PBL code uses these locations differently, but I have not found anything that helps me understand that. And I have found nothing about the PPA firmware location.


I appreciate any and all help.

タグ(2)
0 件の賞賛
返信
1 返信

1,819件の閲覧回数
Pavel
NXP Employee
NXP Employee

See attached .its file. Change the address for loading.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信