How can we sync the newest commits of kernel and u-boot from nxp?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can we sync the newest commits of kernel and u-boot from nxp?

2,654件の閲覧回数
changbaoma
Contributor IV

eg. QorIQ series and i.MX series.

we use QorIQ series and i.MX series in our project, and use the kernel/u-boot acquired from the Yocto years ago. Since that time i think NXP had commited lots of updates.

So how can we keep trace those commits? Can you show we the git or repo?

0 件の賞賛
返信
6 返答(返信)

2,530件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

You could refer to the following u-boot and Linux Kernel from LSDK 20.04 release.

linux_repo_url=https://source.codeaurora.org/external/qoriq/qoriq-components/linux.git
linux_repo_tag=LSDK-20.04-V5.4-update-290520
second_linux_repo_tag=LSDK-20.04-V4.19-update-290520
cryptodev_linux_repo_url=https://source.codeaurora.org/external/qoriq/qoriq-components/cryptodev-linux.git
cryptodev_linux_repo_tag=LSDK-20.04

u-boot

uboot_repo_url=https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.git
uboot_repo_tag=LSDK-20.04-update-290520

0 件の賞賛
返信

2,530件の閲覧回数
changbaoma
Contributor IV

如果我要下载imx6的linux-5.4.y,以下clone命令是否正确?

git clone https://source.codeaurora.org/external/imx/linux-imx -b git.kernel.org/linux-stable/linux-5.4.y

该下载的内核对比.kernel.org的linux-5.4.y有何区别? 是否已经都已经包含nxp imx6的相关修改和commit?

以及上述内核与imx Yocto Project使用的内核三者间是什么关系?

麻烦 wang工作详细解答. 感谢!

0 件の賞賛
返信

2,530件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please create a new thread in https://community.nxp.com/community/imx?tid=community  to discuss i.MX related questions.

0 件の賞賛
返信

2,530件の閲覧回数
changbaoma
Contributor IV

Thank you very much.

1、How about  i.MX6 series's  git and repo?  I think the repo_url you post above is only for QorIQ processor.

I find this  linux-imx - i.MX Linux kernel , is right for imx6?

2、when the  git clone, i find there are two branchs with 4.19:

#git branch -a

remotes/origin/git.kernel.org/linux-stable/linux-4.19.y
remotes/origin/imx_4.19.35_1.x.0

what is the difference between those two branchs?

which is suggested to use with imx6ull?

3、Is there cryptodev_linux version for imx6?

0 件の賞賛
返信

2,530件の閲覧回数
changbaoma
Contributor IV

what are the differences between cryptodev_linux_repo and linux_repo?

0 件の賞賛
返信

2,530件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Cryptodev-linux is a Linux-kernel device that allows user-space access to hardware cryptographic accelerators.

0 件の賞賛
返信