Help needed to deploy image from NXP Yocto BSP for LS1046afrwy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help needed to deploy image from NXP Yocto BSP for LS1046afrwy

1,494 Views
anderstietze
Contributor II

I am using the NXP Yocto Linux BSP SDK for a LS1046afrwy board which i have downloaded from

https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk

I am able to build the "fsl-image-networking" with success, but I cannot find any instructions how to deploy the output image to a SD card.

1) Is there any guide howto deploy the above image to an SD-card?

2) Are there any plans to update the yocto-sdk to the latest LSDK release. Last commit is almost 9 month old?

Thank you.

Tags (1)
0 Kudos
Reply
1 Reply

1,428 Views
Pavel
NXP Employee
NXP Employee

Use solution from the following page:

https://community.nxp.com/message/1292550?commentID=1292550&et=watches.email.thread#comment-1292550

 

NXP offers LSDK for the the LS1046ADRWY board:

https://nxp.flexnetoperations.com/control/frse/download?element=10958497

 

Use this LSDK for image building.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply