Getting Started with the QorIQ LS1046A Reference Design Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Getting Started with the QorIQ LS1046A Reference Design Board

6,064 次查看
marks
Contributor IV

Hello,

A customer just received the LS1046A Reference Design Board and has a few question that I was not able to help with.

Questions:

0. Are there instructions for installing the BSP? I downloaded the file from the NXP website, but the install shell script seems to be referring to an ISO image that I cannot find. The document titled "QorIQ LS1046A BSP v0.4" specifices an ISO image called  "QorIQ-SDK-V2.0-SOURCE-20160527-yocto.iso" and I cant find that.

 1. It looks like there is space for a 2.5” SATA drive in the enclosure. Can I install an SSD like the Samsung 850 PRO 256GB in there? Is there anything special that needs to be done in Linux to use this SSD?

2. The fans are extraordinarily loud! I would like to replace the fans with quieter ones. What is the minimum airflow rate for the RDB?

3. On page 23 of the BSP documentation(cited below),  it mentions an image called “fsl-image-full” as a good place to start. 

 

The file system images contain the programs, scripts, and other files that make up Linux user space. There are five standard images. They are described in the following sections. In the SDK installation directory, look in meta-freescale/recipes-fsl/images for files that define these images. Where to start: “fsl-image-full” contains a rich set of standard Linux features and all special NXP SDK-specific features. It is the best starting point for exploration and evaluation.

Where can I find "fsl-image-full"?

 

Thanks!

Mark

标签 (1)
标记 (1)
0 项奖励
回复
6 回复数

4,668 次查看
ufedor
NXP Employee
NXP Employee

The Linux SDK v2.0 could be downloaded here:

https://nxp.flexnetoperations.com/control/frse/download?element=7726177 

The page contains download links for the "SOURCE" and "IMAGE" ISOs for the AARCH64.

It will be more convenient to process the issue as a Technical Case - could you please create it?

https://community.freescale.com/thread/381898

0 项奖励
回复

4,668 次查看
lzlibra
Contributor I

hi,ufedor

when i open the download page “https://nxp.flexnetoperations.com/control/frse/download?element=7726177”,it jump to my count page.

How can i download the "QorIQ-SDK-V2.0-SOURCE-20160527-yocto.iso"?

0 项奖励
回复

4,668 次查看
ufedor
NXP Employee
NXP Employee
0 项奖励
回复

4,668 次查看
michaelchen_nsb
Contributor II

hi ufedor

In the SDK download page, https://nxp.flexnetoperations.com/control/frse/download?element=7726177  , I can't found the right image for LS1046

In QorIQ Linux SDK v2.0 AARCH64 IMAGE.iso, is it only for LS1043 and LS2080?

0 项奖励
回复

4,668 次查看
ufedor
NXP Employee
NXP Employee

The requested image is in the "Update: QorIQ Linux SDK v2.0-1703"

0 项奖励
回复

4,668 次查看
michaelchen_nsb
Contributor II

hi ufedor, thanks for your quick help,

for USDPAA usage, six files are needed, The user guide I found are aways talking about P4080, could you please list the specific files for LS1046?

I list all the files in SDK

Name Format Size
----------------------------------------------------------------------------------
AQR-G2_v3.1.5-AQR_RevB_AQR107_ID16068_VER385.cld CLD 282.002 KB
aq_programming.bin BIN 176.703 KB
byte_swap.tcl TCL 1.156 KB
fsl-image-core-ls1046ardb-20170329165208.rootfs.ext2.gz GZ 33.820 MB
fsl-image-core-ls1046ardb-20170329165208.rootfs.ext2.gz.u-boot U-BOOT 33.820 MB
fsl-image-core-ls1046ardb.ext2.gz GZ 0 Byte
fsl-image-core-ls1046ardb.ext2.gz.u-boot U-BOOT 0 Byte
fsl_fman_ucode_ls1046_r1.0_106_4_18.bin BIN 31.840 KB
fsl_fman_ucode_ls1046_r1.0_108_4_9.bin BIN 36.680 KB
Image 0 Byte
Image--4.1-r0-fsl-ls1046a-rdb-20170329165208.dtb DTB 25.093 KB
Image--4.1-r0-fsl-ls1046a-rdb-usdpaa-20170329165208.dtb DTB 26.490 KB
Image--4.1-r0-ls1046ardb-20170329165208.bin BIN 11.834 MB
Image-fsl-ls1046a-rdb-usdpaa.dtb DTB 0 Byte
Image-fsl-ls1046a-rdb.dtb DTB 0 Byte
Image-ls1046ardb.bin BIN 0 Byte
kernel-fsl-ls1046a-rdb-20170329174626.itb ITB 39.080 MB
kernel-fsl-ls1046a-rdb-usdpaa-20170329174626.itb ITB 39.081 MB
kernel-fsl-ls1046a-rdb-usdpaa.itb ITB 0 Byte
kernel-fsl-ls1046a-rdb.itb ITB 0 Byte
modules--4.1-r0-ls1046ardb-20170329165208.tgz TGZ 2.818 MB
modules-ls1046ardb.tgz TGZ 0 Byte
ppa-ls1046ardb-20170329165208.itb ITB 78.940 KB
ppa.itb ITB 0 Byte
README 1.938 KB
rcw_1200_qspiboot.bin BIN 168 Byte
rcw_1400_qspiboot.bin BIN 168 Byte
rcw_1600_emu_qspiboot.bin BIN 160 Byte
rcw_1600_qspiboot.bin BIN 168 Byte
rcw_1600_qspiboot_emmc.bin BIN 168 Byte
rcw_1600_qspiboot_ep.bin BIN 168 Byte
rcw_1600_qspiboot_sben.bin BIN 160 Byte
rcw_1800_qspiboot.bin BIN 168 Byte
rcw_1600_qspiboot.bin BIN 200 Byte
u-boot-emmc-2016.09+fslgit-r0.bin BIN 732.691 KB
u-boot-emmc.bin BIN 0 Byte
u-boot-ls1046ardb.bin BIN 0 Byte
u-boot-qspi-2016.09+fslgit-r0.bin BIN 629.121 KB
u-boot-qspi-secure-boot-2016.09+fslgit-r0.bin BIN 603.801 KB
u-boot-qspi-secure-boot.bin BIN 0 Byte
u-boot-qspi.bin BIN 0 Byte
u-boot-sdcard-2016.09+fslgit-r0.bin BIN 732.691 KB
u-boot-sdcard.bin BIN 0 Byte
u-boot.bin BIN 0 Byte
----------------------------------------------------------------------------------
44 Files - 163.735 MB

0 项奖励
回复