Getting 0x00000101 error code in SCRATCHRW2 while running secure boot on LS1043a

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Getting 0x00000101 error code in SCRATCHRW2 while running secure boot on LS1043a

1,850 次查看
gandhi_999
Contributor III

Hi,

I am trying to run secure boot on LS1043A processor board, however I am not able to see any output in the console after flashing secure pbl and uboot image and using ccs wrote SRKH and OTPMK into fuses.

Then with ccs, I read the SCRATCHRW2 value, and getting error code 0x00000101.

(bin) 23 % ccs::display_mem 32 0x1ee0204 4 0 4
+0 +4 +8 +C
[0x01EE0204] 00000101 00000000 00000000 00000000

I do see the boot holdoff working, and confirmed all registers, etc. 

Could you please help here?

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,784 次查看
kenli
NXP Employee
NXP Employee
0 项奖励
回复