GPU on the LS1028A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPU on the LS1028A

1,451 Views
rhaas
Contributor IV

I am using an LS1028A processor on an avoinics product. We do not need the GPU for the current project. I plan on turning off the GPU using a PBI command.

My question is about verifying if the GPU is actually off. Can you suggest a mechanism I can use to verify the GPU is actually off. This is needed for certification.

0 Kudos
Reply
1 Reply

1,417 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

There isn't a status flag in hardware but you can disable the GPU by the

Device Disable Register 6 (DEVDISR6) 

It is a R/W register so you can read it to verify that it is disabled.

0 Kudos
Reply