GIC Programming on LS2088A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GIC Programming on LS2088A

2,133件の閲覧回数
burakunaltay
Contributor I

Currently I am trying to configure the Generic Interrupt Controller on a LS2088A board.  Since GIC registers are memory mapped and there is no document regarding the system memory map in LS2088A product page, could anyone provide me information about GIC base address in LS2088A boards ?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,846件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

You can see the base address in the LS208xA dts file

https://github.com/torvalds/linux/blob/master/arch/arm64/boot/dts/freescale/fsl-ls208xa.dtsi

/ {

               compatible = "fsl,ls2080a";

               interrupt-parent = <&gic>;

               #address-cells = <2>;

               #size-cells = <2>;

               gic: interrupt-controller@6000000 {

                              compatible = "arm,gic-v3";

                              reg = <0x0 0x06000000 0 0x10000>, /* GIC Dist */

                                            <0x0 0x06100000 0 0x100000>, /* GICR (RD_base + SGI_base) */

                                            <0x0 0x0c0c0000 0 0x2000>, /* GICC */

                                            <0x0 0x0c0d0000 0 0x1000>, /* GICH */

                                            <0x0 0x0c0e0000 0 0x20000>; /* GICV */

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信