Force PCIe errors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Force PCIe errors

6,587件の閲覧回数
kunal_b
Contributor II

Hi,

With LS1043A, I am using PEX3 controller to make a PCIe link to an endpoint device. In firmware, I am periodically reading PCIe error status registers to count correctable, non-fatal uncorrectable and fatal uncorrectable errors. The PCIe link is good and well configured, so I do not get any errors. I am looking for a way to force atleast one of each error type. Is there a way through firmware (eg- register settings) or by injecting a hardware fault on PCIe link (eg- grounding a PCIe interface line) to force any of these errors?  

Correctable errors- Advisory Non-Fatal Error , Replay timer timeout, REPLAY_NUM Rollover, Bad DLLP, Bad TLP, Receiver error. 

Non-fatal uncorrectable errors- Unsupported request error status, ECRC error status, Unexpected completion status, Completer abort status, Completion timeout status, Poisoned TLP status. 

Fatal uncorrectable errors- Malformed TLP, Receiver overflow, Flow control protocol error, Data link protocol error. 

Thank you

タグ(1)
0 件の賞賛
返信
3 返答(返信)

6,566件の閲覧回数
khushbur
NXP TechSupport
NXP TechSupport

HI @kunal_b 

 

Please refer LSDK 21.08 User Guide section 7.2.8.2 PCIe Advanced Error Reporting User Manual to fake various kinds of PCIe errors.

 

Thanks

Khushbu

0 件の賞賛
返信

6,553件の閲覧回数
kunal_b
Contributor II

Hi Khushbu,

I am not using LSDK or Linux with LS1043A. I am using bare-metal programming. I saw that the LSDK user guide section 7.2.8.2 uses a software tool to inject PCIe error. Can you let me know what the tool does? Is it an intrusive error injection technique which injects error in PCIe controller's dataflow or some simple PCIe register settings? I am trying to understand if I can replicate the tool's behavior in bare-metal programming.

Thank you

-Kunal 

0 件の賞賛
返信

6,517件の閲覧回数
khushbur
NXP TechSupport
NXP TechSupport

Hi @kunal_b 

 

Please refer below link for more information about aer-inject test utility

https://www.kernel.org/doc/Documentation/PCI/pcieaer-howto.txt

 

Thanks

Khushbu

0 件の賞賛
返信