Firmware burn write step command line instruction

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Firmware burn write step command line instruction

ソリューションへジャンプ
1,421件の閲覧回数
Kevin06
Contributor I

LS1046A uses CodeWarrior to burn firmware on the Windows platform. The bare board connects to the PC through CodeWarrior TAP and hopes to perform the burn steps in the command line mode. How to write the command line instruction of the above burning function?

0 件の賞賛
返信
1 解決策
1,393件の閲覧回数
June_Lu
NXP TechSupport
NXP TechSupport

You could use flash programmer to recovery the board. You could find the user case from C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\Help\PDF\ARMv8_Targeting_Manual, page 140, if the customer board support RCW override. If not , please use Hard-Code RCW.

It is recommended to disconnect RESET_REQ_B from PORESET_B when recovery the board.

For the flash commands, please refer to C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\Help\PDF\ARMv8_Targeting_Manual, page 96.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,394件の閲覧回数
June_Lu
NXP TechSupport
NXP TechSupport

You could use flash programmer to recovery the board. You could find the user case from C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\Help\PDF\ARMv8_Targeting_Manual, page 140, if the customer board support RCW override. If not , please use Hard-Code RCW.

It is recommended to disconnect RESET_REQ_B from PORESET_B when recovery the board.

For the flash commands, please refer to C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\Help\PDF\ARMv8_Targeting_Manual, page 96.

0 件の賞賛
返信